Solution


Verification Test Stand

Customer is looking for a way to verify if the load cell is in “good working order” for an upcoming test.


Summary

  • Customer Need / Challenge

    Customer is looking for a way to verify if the load cell is in “good working order” for an upcoming test.

  • Interface Solution

    Interface proposed a solution with the customer’s supplied verification load frame, Model 1210 Precision LowProfile® Load Cell, connected with Model SI-USB4 4-Channel USB Interface Module.

  • Results

    Customer installed their load cell and Model 1210 Precision LowProfile® Load cell into the verification load frame, and applied forces were displayed and recorded by Model SI-USB4 4-Channel USB Interface Module for review and record keeping on customer’s computer.

Materials


  • 1210 Precision LowProfile® Load Cell
  • SI-USB4 4-Channel USB Interface Module with included setup, logging, and graphing software
  • Customer’s verification load frame
  • Customer’s test load cell
  • Customer’s supplied PC computer

How it Works


  1. Customer installed their load cell to the customer’s verification load frame, connecting it to 1210 Precision LowProfile® Load Cell.
  2. Customer applied the specific load by turning the manual actuator.
  3. Applied forces were measured by the 1210 Precision LowProfile® Load Cell.
  4. Results from the load cell under test and from the 1210 Precision LowProfile® Load cell were displayed and recorded by the SI-USB4 4-Channel USB Interface Module for review and record keeping on customer’s computer.

Download PDF


Animated Application Note